Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Meaning of Wakeup Pulse Filter Constant in S6BT112A - KBA228428

Meaning of Wakeup Pulse Filter Constant in S6BT112A - KBA228428

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: AtsushiT_61           Version: **

Translation - Japanese: S6BT112Aのウェイクアップ パルス フィルター定数の意味 - KBA228428 -

Question:

What is the meaning of the wakeup pulse filter constant in S6BT112A?

Answer:

At the Master Node: In the wakeup pulse of the Sleep mode, the transceiver is designed so that a low pulse less than the Trx_wakeup_master value input to the BUS pin is not output to the RXD pin. The RXD pin waveform is delayed by 30 to 150 us with respect to the bus waveform.

At the Slave Node: In the wakeup pulse of the Sleep mode, the transceiver is designed so that a low pulse less than the Trx_wakeup_slave value input to the BUS pin is not output to the CLK pin. The CLK pin waveform is delayed by 0.5 to 5 us with respect to the bus waveform.

Table 1 lists the wakeup pulse filter constant and Figure 1 shows the filtered waveforms at wakeup. For more details, see Table 8-7. AC Characteristics in the S6BT112A datasheet.

Table 1. Wakeup Pulse Filter Constant

Parameters

Symbol

Pin Name

Conditions

Min

Typ

Max

Unit

Wakeup pulse filter constant (Master)

Trx_wakeup_master

BUS

NSLP = 0 V

SELMS = 0 V

VTH(bus) = 42.3 %

30

-

150

us

Wakeup pulse filter constant (Slave)

Trx_wakeup_slave

BUS

NSLP = 0 V

SELMS = 5 V

VTH(bus) = 42.3 %

  1. 0.5

-

5

us

Figure 1. Filtered Waveforms at Wakeup

pastedImage_0.png

0 Likes
242 Views
Contributors