Manufacturer's Part Number (MFR#): Meaning of the last character
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
What does the last (18th) character mean in the MFR# id number on the packaging label?
Example:
The last character in the MFR# is for internal Infineon use and has no meaning for customers.
The sample packaging label shows two numbers and a bar code:
- The first number is the 17-character Ordering Part Number (OPN) that is specified in the datasheet for the Infineon's part.
- The second number is the Manufacturing Part Number (MFR#) which consists of the OPN plus an additional character.
- The last (18th) character is a code that is used for Infineon’s internal tracking purposes; it has no meaning for the recipient.
- The 18th character has no bearing on the form, fit, function, and operation of Flash, and has no impact on the options selected by the OPN.
When ordering Infineon's products, the 18th character is not required. Although the MFR# may be found on associated documents, labels, and so forth, the MFR# is not stamped on the chip.
Here are sample MFR#s for three different OPNs:
S25FL116K0XMFI043Z (MFR# = OPN + Z)
S29AL016J70TFI010A (MFR# = OPN + A)
S29JL032H70TFI320H (MFR#= OPN + H)
- Tags:
- 0’s
- 1’s
- alpha
- ambient
- architecture
- bank
- beta
- bga
- bit-flip
- block
- bottom boot
- buffer
- byte mode
- capacitor
- cfi
- chip
- command
- common flash interface
- confidence level circuit
- cosmic
- current
- cycle
- decoupling
- definitions
- delay
- density
- device id
- divider
- erase resolution
- error
- exposure
- failure
- filter
- float
- floating gate
- full block
- gamma
- half block
- hard error
- hex
- hyperbus
- hyperflash
- hyperram
- interface
- junction temperature
- keywords: technology
- latency
- length
- manufacturers id
- mcp
- memory
- mirrorbit
- mode
- multi plane
- nand
- neutron
- nor
- one’s
- open
- operation
- package
- page
- parallel
- parallel nor
- pc board
- pcb
- plane
- printed circuit board
- program
- pull down
- pull up
- radiation
- read
- resistor
- routing
- s25fl064l
- s25fl116k
- s25fl127s
- s25fl128l
- s25fl132k
- s25fl164k
- s25fl256l
- s25fl256s
- s25fl512s
- s25fs064s
- s25fs128s
- s25fs256s
- s25fs512s
- s25fs512t
- s26kl128s
- s26kl256s
- s26kl512s
- s26ks128s
- s26ks256s
- s26ks512s
- s27kl0641
- s27ks0641
- s29al008j
- s29al016j
- s29as008j
- s29as016j
- s29gl01gp
- s29gl01gs
- s29gl01gt
- s29gl032n
- s29gl064s
- s29gl128p
- s29gl128s
- s29gl256p
- s29gl256s
- s29gl512p
- s29gl512s
- s29gl512t
- s29jl032j
- s29jl064j
- s29pl032j
- s29pl064j
- s34ml01g2
- s34ml02g2
- s34ml04g2
- s34ml08g2
- s34ml16g2
- s34ms01g2
- s34ms02g2
- s34ms04g2
- s34ms08g2
- s34ms16g2
- s70fl01gs
- s70fs01gs
- s98
- s99-
- sector
- sector block
- sector erase
- serial
- serial nor
- set
- seu
- short
- simultaneous
- single event upset
- single level cell
- size
- slc
- slc nand
- soft error
- software reset
- soic
- spare area
- spi
- status reliability
- storage
- subsector
- thermal resistance
- top boot
- trace
- tsop
- unconnected
- uniform
- uson
- voltage divider
- word mode
- write buffer
- wson
- x-ray
- zero’s