What is the meaning and purpose of AEC-Q100?
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
The AEC-Q100 standard is a set of rigorous requirements and tests that electronic components must pass to ensure their suitability for use in automotive applications. Since the automotive industry requires electronic components that can perform reliably in harsh environments and under demanding conditions, the AEC-Q100 is an industry standard specification that helps to ensure the quality and reliability of electronic components used in automotive applications.
The AEC-Q100 standard is widely recognized and adopted in the automotive industry and is an important consideration in the design and manufacturing of electronic components for automotive applications.
Role of AEC-Q100:
AEC-Q100 standard plays a critical role in ensuring the safety and reliability of automotive products and helps to drive innovation and progress in the automotive industry.
AEC-Q100 is a set of qualification test sequences for integrated circuits developed by the Automotive Electronics Council (AEC). AEC-Q100 establishes common part-qualification and quality-system standards for automotive electronics, and is the industry-standard specification that outlines the recommended new product and major change qualification requirements and procedures for packaged integrated circuits embedded into automotive applications.
Find out more about AEC-Q100 specifications here!.
Products that are qualified for automotive applications meet the AEC-Q100 requirements and may be labelled with the following automotive temperature grades in Table 1.
Table 1 - Automotive Electronics Council Temperature Grades
Grade |
Ambient operating temperature range |
0 |
-40°C to +150°C |
1 |
-40°C to +125°C |
2 |
-40°C to +105°C |
3 |
-40°C to +85°C |
Note: There are currently Grade-1, Grade-2, and Grade-3 as AEC-Q100 ordering options.
Translation from Japanese: AEC-Q100の意味 – KBA220733 - Community Translated (JA)
- Tags:
- a25l
- a25lq
- a29
- a290
- a29l
- adesto
- aec-q100
- aecouncil
- ambient
- amic
- applications
- at25bcm
- at25df
- at25dl
- at25dn
- at25dq
- at25f
- at26df
- at45db
- automotive
- automotive electronics council
- Automotive Electronics Council (AEC)
- Automotive Temperature Grades
- competitor
- cypress flash memory products
- definition
- embedded
- en25b toshiba
- en25f
- en25p
- en25q
- en25qh
- en29gl
- en29lv
- en39sl
- es29lv
- esi
- esmt
- f25l
- f25s
- f49l
- gd25q
- gigadevice
- grade
- integrated circuits
- is25cq
- is25ld
- is25lq
- issi
- jr28f
- js28f
- jz58f
- k8a
- k8c
- k8d
- k8f
- k8p
- k8q eon
- m25p
- m25pe
- m25px
- m28w
- m29dw
- m29f
- m29w
- m36a
- m36l
- m36w
- m39l
- m58bw
- m58l
- m58w
- macronix
- micron
- mx25l
- mx25v
- mx29f
- mx29gl
- mx29lv
- mx29sl
- mx66l
- n25q winbond
- nor
- operating temperature
- parallel nor
- pc28f
- pf38f
- pf48f
- pf58f
- procedures
- pz28f
- Q25g
- qualification
- range
- rc28f
- rd48f
- s25fl064l
- s25fl116k
- s25fl127s
- s25fl128l
- s25fl132k
- s25fl164k
- s25fl256l
- s25fl256s
- s25fl512s
- s25fs064s
- s25fs128s
- s25fs256s
- s25fs512s
- s25fs512t
- s29al008j
- s29al016j
- s29as008j
- s29as016j
- s29gl01gp
- s29gl01gs
- s29gl01gt
- s29gl032n
- s29gl064s
- s29gl128p
- s29gl128s s29gl256s
- s29gl256p
- s29gl512p
- s29gl512s
- s29gl512t
- s29jl032j
- s29jl064j
- s29pl032j
- s29pl064j
- samsung
- serial nor
- specifications
- tc58nvg2s0hbai4
- te28f
- w25q
- w25x
- w29gl
- °c