Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Maximum Ripple voltage in PSoC Power Supply

Maximum Ripple voltage in PSoC Power Supply

Anonymous
Not applicable
Question: What is the maximum ripple voltage that we should consider on hardware design?

 

Answer:

There isn't any thumb rule on maximum ripple voltage. When CPU is operated at 24MHz, the PSoC's VDD has to be greater than 4.75V. The ripple content in the supply should be low enough such that the voltage does not droop below 4.75V. Also, for better analog performance it would be better to have the least ripple.

Refer the device specific datasheets for any specific constraints on the supply voltage.

0 Likes
203 Views
Contributors