Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

LIN mode wrong for slow VS rise time in TLE9879 power-up sequence test

LIN mode wrong for slow VS rise time in TLE9879 power-up sequence test

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: TLE9879のパワーアップシーケンステストで、VSの立ち上がり時間が遅い場合にLINモードが正しくない (KA-01395)

In the car, we expect every possible voltage slope (VS) and transition. Even slower slopes should not have an influence on the functionality. When voltage slope transitions are slow during power up sequence test, if the transceiver is in LIN Normal Mode (LNM) instead of LIN Receive Mode (LROM), VS under voltage can be triggered, which causes the LIN to go in Receive-only mode.
LNM to LROM transition is also executed when:
- MODE is configured to LIN Receive-Only Mode or
- Feedback signals of Mode and Slope Mode are not ok or
- VS undervoltage flag (VS_UV_STS) is set or
- LIN transceiver OT_STS or OC_STS are set or
- TXD_TMOUT is set
LROM to LNM transition is executed when:
- MODE is configured to LIN Normal Mode and
- Feedback signals of Mode and Slope Mode are ok and
- VS undervoltage flag (VS_UV_STS) is not set and
- LIN transceiver OT_STS and OC_STS are not set and
- no TXD_TMOUT is set
For further information, please refer to the TLE987xQX User Manual (Page 651) under https://www.infineon.com/cms/en/product/microcontroller/embedded-power-ics-system-on-chip-/3-phase-b... User Manual.

0 Likes
209 Views