Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

L2CAP Connection Parameters for Apple Devices

L2CAP Connection Parameters for Apple Devices

Anonymous
Not applicable

What are the conditions to be met while setting the connection parameters for Apple devices?

 

The peripheral must take care of the parameters used for low-energy connection. The peripheral should request connection parameters appropriate for its use case by sending an L2CAP Connection Parameter Update after the connection is established.

The connection parameter request should meet the following conditions:

● Maximum Connection Interval × (Slave Latency + 1) ≤ 2 seconds

● Minimum Connection Interval ≥ 20 ms

● Minimum Connection Interval + 20 ms ≤ Interval Maximum Slave Latency ≤ 4

● Connection Supervision Timeout ≤ 6 seconds

● Maximum Connection Interval × (Slave Latency + 1) × 3 < Connection Supervision Timeout

If a Bluetooth Low Energy human interface device (HID) is one of the connected services of an accessory, connection interval down to 11.25 ms may be accepted by the Apple product.

 

Version: *A

Translation - Japanese: Appleデバイス用のL2CAPコネクションパラメータ– KBA203284- Community Translated (JA)

0 Likes
801 Views