Key benefits of the TO-247PLUS 4pin package for 1200 V IGBT
Community Manager
Jun 01, 2022
12:49 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jun 01, 2022
12:49 AM
Community Translation: 1200V IGBT TO-247PLUS 4pin パッケージの主な利点
- 20% reduction of turn on losses due to better feedback loop to driver IC with 4th pin Kelvin Emitter package configuration
- Higher system power density - Ic increase from 40A up to 75A 1200V keeping the same system thermal performance
- 20% lower thermal resistance Rth(jh) and improved by ~15% heat dissipation capability of TO-247PLUS vs TO-247.
Labels
Rate this article: