Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Inverting the Display on a 16x2 Character LCD in PSoC® Creator™ Design - KBA203635

Inverting the Display on a 16x2 Character LCD in PSoC® Creator™ Design - KBA203635

Anonymous
Not applicable

Version: **

Translation - Japanese: PSoC® Creator™ のデザインで 16x2 Character LCD の表示を反転させる - KBA203635 - Community Translated (JA)

Question:

How do I invert the display (toggle dots which are ON to OFF, and vice-versa) on a 16x2 character LCD interfaced with PSoC 3/ PSoC 5LP using PSoC Creator?

Answer:

You can use the custom character set of the LCD and create your own symbols, as shown in the diagram below:

1.png

However, you have only a limited set of characters in the custom character map. In addition, you cannot directly control the pixels because they are handled by the driver IC inside the LCD module. As a workaround, consider using a graphic LCD where you can control pixels on the display.

0 Likes
567 Views
Contributors