Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Interrupt number in PSoC™ Creator - KBA236407

Interrupt number in PSoC™ Creator - KBA236407

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted

Community Translation: PSoC™ Creator の割り込み番号 – KBA236407

Version: **

An instance of component which needs to use a system interrupt is assigned an Interrupt Number in the Interrupts tab of the *.cydwr window of PSoC™ Creator, as shown in the following figure.

Infineon_Team_0-1665749071512.png

Figure 1 Interrupt number in PSoC™ Creator

The interrupt IRQx from a peripheral is represented by x.  For example, in the above figure, the number 13 means the interrupt IRQ13 for the device, and the number 7 is for IRQ7. PSoC™ Creator uses this number to map the interrupts of peripherals to CPU exceptions number. For more details, see Interrupts chapter in the architecture TRM of each PSoC™ family.

0 Likes
215 Views