Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Interfacing PSoC® 1 to an SPI EEPROM – KBA221411

Interfacing PSoC® 1 to an SPI EEPROM – KBA221411

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: **

Translation - Japanese: PSoC®1とSPI EEPROMのインターフェース – KBA221411 - Community Translated (JA)

Question:

How do I interface PSoC® 1 to an external SPI EEPROM?

Answer:

The attached project demonstrates how PSoC® 1 may be interfaced to an external SPI EEPROM and an ATMEL AT25080A device. In the project, PSoC communicates with the external SPI EEPROM using the SPI Master (SPIM) User Module. An array of 32 bytes is written to the EEPROM starting from location 0 to 31 and the same array is read back from the EEPROM. The first eight bytes read back are displayed on the LCD.

The attached document provides complete information on the user modules, their placement, User Module parameter settings, Global Resources settings, and the hardware connections. It also provides a detailed description on the working of the project.

Download the documents and project files from the following links:

0 Likes
207 Views
Contributors