Input Tolerance of CY2304NZ
Anonymous
Not applicable
Dec 19, 2008
12:00 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Dec 19, 2008
12:00 AM
Question: Is CY2304NZ input 5V tolerant?
Answer:
The input of CY2304NZ non zero delay buffer device is not 5V tolerant. Due to the input clamping diode, the input needs to be less than VDD + 0.5V. So the Input needs to be < 4.1V (=3.6 + 0.5), according to datasheet.
- Tags:
- clock distribution
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous