Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Input Rise and Fall Times of CY2309 - KBA219626

Input Rise and Fall Times of CY2309 - KBA219626

Anonymous
Not applicable

Version: **

Translation - Japanese: CY2309の入力立ち上がり時間と立ち下がり時間 - KBA219626 - Community Translated (JA)

Question:

Are there any rise or fall time restrictions on the input of the CY2309 low-cost 3.3-V Zero-Delay Buffer? Are there any Schmitt Triggers on the inputs?

Answer:

There is no restriction on the rise or fall times on the input of CY2309. The device uses regular CMOS input buffers that trigger when the input pass the Vdd/2 threshold. There are no Schmitt triggers on the inputs.

0 Likes
281 Views
Contributors