In which topologies can CoolMOS™ S7 be used?
Community Manager
Jul 03, 2022
11:17 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jul 03, 2022
11:17 PM
Community Translation: CoolMOS™ S7 はどのようなトポロジーで使用できますか?
Theoretically in any topology leg switching at low or grid frequency, plus in all solid state solutions.
Examples are:
1. Classic PFC, interleaved PFC and boost PFC all can use CoolMOS™ S7 in parallel to diodes for rectification purposes, obtaining a boost in efficiency
2. Another example is the CCM totem-pole PFC, where CoolMOS™ S7 is suitable for the low-switching leg of the bridge, becoming the perfect complement to CoolSiC™ MOSFETs and CoolGaN™ HEMTs.
Labels
- Tags:
- CoolMOS S7
- topologies
Rate this article: