cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

IO pins active with the monitor running after downloading a firmware program from Keil

Anonymous
Not applicable

IO pins active with the monitor running after downloading a firmware program from Keil

Question: After downloading a firmware program from the Keil IDE and it's running the little monitor routine, Which IO pins will be active with the monitor running?

 

Answer:

The monitor that is downloaded automatically on start up  is mon-ext-sio1-e0.hex (for EZ-USB and EZ-USB FX).  This monitor uses serial port 1 (SIO-1) to talk to the device.  PORTB pins, bit 2 and bit3 are  used for RxD1 and TxD1 for receiving and transmitting data respectively.  Hence PORTB pins 2 and 3 are dedicated for their alternate functions and are not available as general purpose I/O.If you are using the monitor that uses SIO-0, RxD0 and TxD0 are alternate functions on PORTC bits 0 and 1 respectively. PORTC pins 0 and 1 are no more available for general purpose I/O

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Dec 19, 2008 12:00 AM
Updated by:
Anonymous
 
Contributors