cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Hysteresis on Input of Cypress Quantum38K CPLDs

Anonymous
Not applicable

Hysteresis on Input of Cypress Quantum38K CPLDs

Question: Do Quantum38K CPLDs have hysteresis on the inputs?

 

Answer:

Quantum38K CPLD's do not have explicit input hysteresis, but the effect of the bus hold circuit (if enabled) on the input may look like hysteresis. Bus hold can be approximated as a current source. As the input rises, bus hold will continue to pull low. Eventually, the input reaches the bus hold trip point and the output changes state. That means it switches from pulling low to pulling high. This change in direction of the bushold current together with the output impedance of the driver will cause a "jump" in the input voltage which looks a lot like hysteresis.

Please be noted our entire Cypress CPLD product are Obsolete and not recommended for new design and development. For more information on CPLD product, please visit our webpage: http://www.cypress.com/go/cpld

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jan 01, 2012 05:10 PM
Updated by:
Anonymous
 
Contributors