Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

HyperBus Interface Channel Selection – KBA223297

HyperBus Interface Channel Selection – KBA223297

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: **

Translation - Japanese: ハイパーバスインターフェースチャネル選択 - KBA223297 - Community Translated (JA)

Question: In the S6J3200 SampleSW hyperbusi example, why is the HyperBus interface ch.0 type (HYPERBUSI0_Type) used for the GPOR register configuration when selecting ch.1?

Answer: HyerBus interface ch.0 (for MCU) and ch.1 (for Graphic) are assigned to the same GPIO pins. To select ch.0 or ch.1, the GPO bit of the HYPERBUSIn_GPOR register should be configured and only the HYPERBUSIn_GPOR register in HyperBus ch.0 is used. When you select HyperBus interface ch.1, the example uses HYPERBUSI0_Type to configure the GPOR register.

The bit and function for channel selection are as follows:

GPO[0]

Description

0

Select HyperBus Interface Ch. 0

1

Select HyperBus Interface Ch. 1

Notes:

  • GPO[1] in HYPERBUSIn_GPOR of HyperBus Interface Ch. 0 is not used.
  • GPO[1:0] in HYPERBUSIn_GPOR of HyperBus Interface Ch. 1, Ch.2 are not used.
  • If HyperBus Interface Ch.2 is used, the configuration of the GPO bit is unnecessary.

  1. Example.

            //Config HyperBus Ch.1

            Hyperbusi_Init(HYPERBUSI1_Type, &HyperbusiConf);

            Hyperbusi_SetGPOutput(HYPERBUSI0_Type, HyperbusiLowPolarity, HyperbusiHighPolarity);

For more information about the HyperBus Interface, refer to the S6J3200 Hardware Manual.

254 Views
Contributors