Community Manager
Nov 24, 2021
04:36 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Nov 24, 2021
04:36 AM
How to select the inductor for an LED driver application in boost to ground topology
Two equations are needed to choose the correct value of inductor for the DC-DC
- The first equation determinates the minimum inductance Lmin as a function of the input and output voltages VIN and VOUT as well as the switching frequency fsw and the ripple current ΔIL:
Lmin ≥ (VOUT-VIN)/VOUT * VIN/(ΔIL * fsw)
- The second equation gives the minimum inductance to prevent discontinuous conduction mode (DCM) as a function of the maximum input voltage VIN_MAX and the minimum input current IIN_MIN:
Lmin ≥ (VOUT-VIN)/VOUT * VIN_MAX/(2*IIN_MIN * fsw)
For further information check the TLD5099EP datasheet, while more information on how to design a proper solution can be found in the Z8F66213399 DRL driver with TLD5099EP B2G-AN application note
Labels
Rate this article: