How to resolve debugger connection error in TRAVEO II Family MCU - KBA233438
Employee
Jul 12, 2021
10:34 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jul 12, 2021
10:34 PM
Version: **
Question: What needs to be checked if JTAG debugger is not connected?
Answer: If the signal quality of the hardware is not good, do the following:
- Make sure that the JTAG signal wiring on the PCB meets the requirements.
- Check if the JTAG termination circuit is appropriate.
For more information, see the documentation as follows.
AN220270 Hardware Design Guide for the TRAVEO II Family
AN220118 Getting Started with TRAVEO II Family MCUs
Note: This KBA applies to the following series of TRAVEO™ II MCUs:
- CYT2 Series
- CYT3 Series
- CYT4 Series
Labels
Rate this article: