How to do fade in/out functions without MCU using LITIX Power LED drivers?
Community Manager
Nov 25, 2021
01:58 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Nov 25, 2021
01:58 AM
With LITIX Power boost controllers it is possible to implement a delay and fade-in / fade-out functions without using a microcontroller.
This can be done by using filters with different time constant at the SET pin. The SET pin is the analog adjustment input and it is used to control the output current. One of the filters needs to be switchable.
In the example below
- Filter 1 is a low pass filter that enables and disables the output current with a defined delay by closing or opening the MOSFET
- Filter 2 is a low pass filter that enables the fade-in/fade-out function.
See our LITIX web pages for more information on our automotive LED drivers
Labels
Rate this article: