Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

How should unused pins of LITIX Basic+ be connected when all of outputs will not be used?

How should unused pins of LITIX Basic+ be connected when all of outputs will not be used?

IFX_Publisher1
Community Manager
Community Manager
Community Manager
250 sign-ins First comment on KBA 250 replies posted

When one output channel of TLD2331-3EP is not used, you should leave the IN_SETx pin open as well as the corresponding output, OUTx. If SLS detection is required, it is recommended to use output 2, OUT2, since this is used as reference for the SLS detection threshold (leave one of the remaining outputs open, OUT1 or OUT3).
When one output channel of the TLD2131-3EP or TLD2142-3EP is not used, you should connect to the unused output a diode chain or a Zener. If TLD2131-3EP is required to detect SLS, then use OUT2 and leave OUT1 or OUT3 open.

0 Likes
129 Views