Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

How should the VEE2 pin in the1ED38x0Mc12M Enhanced be connected?

How should the VEE2 pin in the1ED38x0Mc12M Enhanced be connected?

IFX_Publisher4
Employee
Employee
50 questions asked First comment on KBA First reply posted
The VEE2 is basically the negative supply terminal of the output side of the gate driver. It should be connected to a voltage between 0 V to -25 V referenced to GND2 for proper operation. If there is no negative voltage used then make sure that all VEE2 pins are connected to GND2.
0 Likes
62 Views
Contributors