Community Manager
Nov 25, 2021
12:51 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Nov 25, 2021
12:51 AM
How many LITIX™ BASIC+ LED drivers can be used for one function to meet <10 mA fault mode current?
In total you can use up to 11 LITIX™ BASIC+ LED driver devices for one function on the same ERRN bus.
Rationale:
Referring to the ECs (Electrical Characteristics) "internal supply and EN pin" two parameters are of interest:
- IS(fault,ERRN): Current consumption during fault condition triggered from another device sharing ERRN bus (all channels deactivated) is < 0.85 mA
- IS(fault,OUT) Current consumption during fault condition (all channels deactivated) is < 1.25mA
So in total you can use 11 devices in one function since 1.25mA+(11-1)*0.85mA=9.75mA<10mA.
Find the datasheets and application notes at https://www.infineon.com/cms/en/product/power/lighting-ics/litix-automotive-led-driver-ic/litix-basi...
Labels
Rate this article: