How do I calculate the temperature derating for NOR flash? –KBA234993
Community Manager
Mar 23, 2022
10:01 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Mar 23, 2022
10:01 PM
Community Translation: NORフラッシュの温度ディレーティングを計算するにはどうすればよいですか? - KBA234993
Version: **
Question: Why is the Junction temperature not specified in the datasheet? How do I calculate the temperature derating for NOR flash?
Answer: Junction temperature is not specified in the datasheet for NOR flash devices because a memory device does not draw a high amount of power like a controller or power device. In addition, Infineon flash memories do not have a large variation of operating conditions that have significantly different power draws; therefore, you can ignore the core temperature and derating considerations. Set the ambient temperature at or below the temperature specified for the device in the datasheet.
Labels
- Tags:
- datasheet
- fl-l
- fl-p
- fl-s
- fs-s
- GL-N
- gl-p
- gl-s
- gl-t
- hl-t
- hs-t
- hyperflash
- junction temperature
- kl-s
- ks-s
- nor flash
- parallel
- pl-j
- power consumption
- serial
- spi
- VS-R
Rate this article: