Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Knowledge Base Articles

High Z parameters for some SRAM's clarifications

Anonymous
Not applicable

High Z parameters for some SRAM's clarifications

Translation - Japanese: 特定のSRAMのHigh-Zパラメータについて- Community Translated (JA)

Question: tHZWE for some speed grades -15, -20, -25 is specified less than tLZWE. Is this correct?

Answer:

Yes, this is correct. Note #7 on the datasheet, which states that tHZWE is less than tLZWE at any given temperature and voltage range. On some of our Fast Asynchronous datasheets, the value for tLZWE is less than that of tHZWE, but tLZWE is always specified as a min, while tHZWE is specified as a max. Over the course of normal operation, tHZWE should be less than that of tLZWE.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Mar 26, 2011 12:32 AM
Updated by:
Anonymous
 
Contributors