Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Handling Unused Pins of Traveo™ S6J3XXX/CY9D560 Series MCUs - KBA213943

Handling Unused Pins of Traveo™ S6J3XXX/CY9D560 Series MCUs - KBA213943

Anonymous
Not applicable

Version: *C

Translation - Japanese: Traveo™ S6J3XXX/CY9D560 シリーズ MCU の未使用ピンの処理について - KBA213943 - Community Translated (JA)

Question:

What is the recommendation for terminal setting of unused GPIO pins?

Notes:

1.This KBA applies to the following series of Traveo MCUs:

S6J3110

S6J3120

S6J3200

S6J3300

S6J3350

S6J3360

S6J3370

S6J3400

S6J3510

CY9D560

2.Product prefix "MB" has been changed to "CY".

Answer:

Leaving unused input pins open may cause permanent damage from a malfunction or latch-up. Take measures for unused pins such as pulling up or pulling down the voltage with resistors of 2 kilo ohms or higher.

If there are any unused input/output pins, set them to the output state and then open them, or set them to the input state and handle them in the same way as input pins.

649 Views