Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Graphics Subsystem in Traveo S6J3200 MCU - KBA225719

Graphics Subsystem in Traveo S6J3200 MCU - KBA225719

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: kotaroh_86           Version: **

Translation - Japanese: タイトル:Traveo S6J3200 MCUのグラフィックサブシステム – KBA225719- Community Translated (JA)

Question 1: Is there any penalty or bandwidth constraint between Display Controller 0 and Display Controller 1 in the graphics subsystem of Traveo™ S6J3200 MCU?
Answer 1: There is no constraint from the software and graphics point of view. However, there are differences between the physical pins on the MCU. Display Controller 0 can drive higher pixel clock (80 MHz) compared to Display Controller 1 (50 MHz). Also, Display Controller 0 pins have higher drive strength.

Question 2: Can Display Controller 0 and Display Controller 1 support DRGB888, RSDS, and LVDS formats?
Answer 2: Display Controller 0 supports RSDS, DRGB, and LVDS for some part number options. Display Controller 1 supports only DRGB. For more detail, see Chapter 2.2 Optional Function of the S6J3200 Series Datasheet.

Question 3: Does the graphics subsystem of Traveo S6J3200 MCU  support PNG decompression?
Answer 3: No, the graphics subsystem of Traveo S6J3200 MCU does not support PNG decompression.

Question 4: What happens when an unlock function of graphics subsystem is executed more than 15 times?
Answer 4: If an unlock function of graphics subsystem is executed more than 15 times, NMI 20 ‘Graphics subsystem memory protection’ occurs.

Question 5: How can I setup 8 or 16 scanlines mode of 3D Graphics Core?
Answer 5: 3D Graphics driver software supports only four scanlines mode. User applications cannot change the scanline setting.

0 Likes
374 Views
Contributors