Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Global Variables Not working When Used in CY_ISR - KBA224452

Global Variables Not working When Used in CY_ISR - KBA224452

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: JobinT_31        Version: *A

 

Translation - Japanese: CY_ISRで使用するとグローバル変数が機能しない - KBA224452- Community Translated (JA)

 

Question:

Global variables used across the main function and a CY_ISR are not working. Why?

Answer:

At higher levels of optimization, global variables can get optimized out by the compiler. This happens when the variable is modified only by functions like CY_ISR. Use the volatile keyword to inform the compiler not to optimize out similar variables, as shown in the following code snippet from a Cypress Developer Community member, Bob_Marlowe.

Example Code:

uint8 FlagToCheck = FALSE;

CY_ISR(SecHandler)

{

      SecTimer_Stop();

      SecTimer_ReadStatusRegister();

      FlagToCheck = TRUE;

}

int main(void)

{

    CyGlobalIntEnable; /* Enable global interrupts. */

    Timeout_StartEx(SecHandler);

    SecTimer_Start();

    LED_Write(LEDOFF);

    /* Place your initialization/startup code here (e.g. MyInst_Start()) */

    while(!FlagToCheck)

    {

    }

      LED_Write(LEDON);

      while(TRUE)

      {

            CyDelay(100);

      }

}

In this example, if optimization in the compiler is set to higher levels, LED_Write(LEDON) will never get executed; however, with the volatile keyword added, LED_Write(LEDON) will get executed.

1889 Views