Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

GPIF™ II Block of FX3 Is Not Full-Duplex – KBA90742

GPIF™ II Block of FX3 Is Not Full-Duplex – KBA90742

Anonymous
Not applicable
Version: **

 

Question: Can the General Programmable Interface II (GPIF™ II) block of FX3 operate in the full-duplex mode (send and receive data simultaneously)?

 

Answer:

No. The GPIFII block of FX3 can operate in only half-duplex mode. You can either send or receive data at any time.

You can configure it for a maximum of 32-bit data bus width and maximum operating clock of 100 MHz, giving you a peak data throughput of 400 MBps.

0 Likes
249 Views
Contributors