For output current >1A, can I connect in parallel the ISOFACE™ output ports? (KA-01368)
Community Manager
Jun 05, 2022
11:53 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jun 05, 2022
11:53 PM
Any of the 8 outputs of the DO (digital output) ISOFACE™ can be connected in parallel to allow higher current output. Diagnostics should be evaluated consequently because the currents can be shared asymmetrically between the different channels in parallel.
Labels
- Tags:
- "ISOFACE
- digital input
- High Current
- industrial interface
- interface IC
- output switches
- parallel connection "
- switches
Rate this article: