Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Flash Write Fail in CY8C201x0 Devices - KBA85520

Flash Write Fail in CY8C201x0 Devices - KBA85520

Anonymous
Not applicable

Version: *A

Translation - Japanese: サイCY8C201x0デバイスでのフラッシュ書き込みの失敗 - KBA85520プレスタイトル- Community Translated (JA)

Question:

Why does the “write configuration to flash” command fail for CY8C201x0 devices?

Answer:

In some devices, flash write fails at operating voltages below 3.0 V. The primary reason is that the CPU clock frequency decreases at lower operating voltages. As a result, the “flash write” routine takes longer and a watchdog reset occurs before the routine is completed. This issue typically occurs on devices that have relatively fast ILO (even though the ILO is within the datasheet specifications).

Workaround: Because watchdog reset triggers when the sleep timer expires three times, reduce the sleep timer frequency (which is configurable over I2C) to 8 Hz or below (if Vdd < 3.0V) before you store the configuration to flash.

0 Likes
413 Views
Contributors