Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Flash Package Marking is Different From the Ordered OPN – KBA 221133

Flash Package Marking is Different From the Ordered OPN – KBA 221133

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Version: **

Translation - Japanese: Cypress Flash Memoryのパッケージ捺印が注文製品番号(OPN / Ordering Part Number) と異なる件について - KBA221133- Community Tra...

Question:

Why is the flash package marking different from the ordering part number (OPN) I ordered?

Answer:

Flash memory dies are becoming smaller due to continuously shrinking process technology, which leads to tiny package sizes. The small package surface does not allow for readable characters if all OPN characters are used, so some characters are not printed to make the remaining characters large enough to be readable.

Refer to the corresponding ‘Ordering Part Number’ section from the datasheet to see all the valid part number combinations including the package marking.

For example, the ordering part number (OPN) for the S25FL-L is defined as follows:

image-1.png

The valid combinations for the standard part are listed below:

image-2.png

As you can see from the above tables, package marking omits the second character of the speed option, the first and last characters from the package/temperature code, and the character code for packing type.

0 Likes
491 Views
Contributors