Finding the Silicon Revision ID of PSoC® 3 Devices - KBA97755
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Version: **
Question:
Where do I determine the Silicon Revision ID for PSoC® 3 devices?
Answer:
You can find Silicon Revision ID in memory at the address 0x46EC. Follow these steps to view the silicon revision:
Step 1 – Connect PSoC 3 to Computer via USB or MiniProg3
The PSoC 3 device should be connected to the computer using MiniProg3 if using a CY8CKIT-001 development kit. If a CYKIT-030 development kit is being used, the USB programming port may also be used to connect the PSoC 3 device to the computer.
Step 2 – Open PSoC Creator.
Step 3 – Debug Any PSoC 3 Project
Click the Debug button in PSoC Creator, as highlighted in Figure 1.
Figure 1. Debug Button
Step 4 – Open Memory Window
Click Debug > Windows > Memory > 1.
Figure 2. Memory Window
Step 5 – View Address 0x46EC
Address 0x46EC contains the silicon revision ID. This memory address can be viewed in the debugger by entering 0x46EC into the memory window’s address field and pressing enter. A value of 0x04 indicates tapeout 5E, while a value of 0x03 indicates tapeout 5.
Figure 3. Silicon Revision ID
-
This widget could not be displayed.Anonymous