Version: **
CCG3PA is Cypress’s USB Type-C Controller targeted for power adapter and power bank applications. CCG3PA supports various fault protections schemes such as over-voltage, under-voltage and over-current protection. The chip can also support over-temperature protection with an external thermistor on a GPIO routed to internal ADC.
The following fault protection schemes can be implemented in CCG3PA. When a fault is encountered, the port disable state is invoked to prevent the system from damage. The following occur in the port disable state:
OVP is implemented for both Type-C port power roles (source and sink). Overvoltage is a fault condition when VBUS exceeds a preset level. During PD negotiation between port partners, the operational VBUS level is negotiated. After the PD negotiation, CCG3PA monitors VBUS in both source and sink roles. If VBUS exceeds the pre-defined threshold, OVP condition is executed.
CCG3PA has a programmable resistor divider and a dedicated comparator for detecting OVP. VBUS is divided using the resistor divider and is routed to the comparator while the other terminal of the comparator is connected with a reference voltage. If VBUS exceeds the threshold, the comparator trips and an interrupt is generated.
As soon as the OV condition is signaled, the firmware disables the port and re-enables it after a pre-defined time. If the OV condition still exists, it goes through the disable-enable cycle again. This is repeated for a specific number of retries after which the port is temporarily disabled; it can be re-enabled through a hard reset/power cycle or by disconnecting/reconnecting the port partner.
UVP is implemented only for the “source” port power role. UVP is implemented only for the “source” port power role. Undervoltage is a fault condition where VBUS drops below the operational level. After the PD negotiation between port partners, CCG3PA monitors the VBUS level; if VBUS falls below the threshold, a UVP condition is declared.
Similar to OVP, CCG3PA has a dedicated comparator to detect UVP.
The resistor divider provides the divided VBUS which is routed to the comparator while the other terminal of the comparator is the reference voltage. If VBUS drops below the UVP threshold, the comparator trips and an interrupt is generated.
On receiving the UVP signal, the firmware disables the Type-C port and re-enables it after a specified time interval. This cycle of disable-enable is repeated for a specified number of retries after which the port is completely disabled; it can be enabled through a hard reset/power cycle or by disconnecting/reconnecting the sink.
OCP is implemented only for the “source” port power role.
Overcurrent is a fault condition when the current consumption is larger than intended.
During power contract negotiation, current is negotiated between port partners. CCG3PA monitors the current levels, and if it exceeds the threshold level, an OCP condition is declared.
CCG3PA has a dedicated comparator and a low-side current sense amplifier (LSCSA) for OCP detection. An external sense resistor Rsense is placed in series with load.
The Rsense resistor is placed across the CSP pin and GND, while LSCSA senses Vsense across Rsense. This is amplified and routed to the comparator where it is compared with the reference voltage. The reference voltage and amplifier gain are related to the target current.
When the current consumption exceeds the threshold, the comparator trips and the OC fault is signalled.
On receiving the OC fault signal, the firmware disables the Type-C port and re-enables it after a specified time interval. This cycle of disable-enable is repeated for a specified number of tries after which the port is completely disabled and can be enabled only through a hard reset/power cycle or by disconnecting/reconnecting the port partner.
OTP is implemented for both Type-C port power roles (source and sink). CCG3PA requires an external thermistor to enable this protection.
Overtemperature is a fault condition when the temperature of the system exceeds a pre-defined threshold value.
CCG3PA uses an external thermistor to monitor system temperature. A fixed resistor is used along with the thermistor to build a resistor divider circuit. The voltage across the thermistor is routed to CCG3PA over a GPIO, and sensed through the internal ADC.
Reference: See the CCGx Power SDK User Guide.