Failure to Compile Variadic Macro in FR Softune V6 - KBA218954
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Version: **
Translation - Japanese: FR Softune V6でVariadicマクロをコンパイルできない - KBA218954 - Community Translated (JA)
Question:
What are the reasons for failure to compile the Variadic Macro: #define Macro(...) __VA_ARGS__ in FR Softune V6?
Answer:
The variadic macro is a new macro for the C99 standard of C language (ISO/IEC 9899:1999). The compiler of the FR Softune V6 supports ANSI and C90 (ISO/IEC 9899:1990) but not C99. Therefore, the variadic macro definition, as shown below, will fail when compiling in FR Softune V6:
//Eg.
#define MY_DEBUG_LOG(...) (printf(__VA_ARGS__))
#define MY_DEBUG_TRACE(format,...) (printf(format,##__VA_ARGS__))
For more information about the supported C/C++ language standards, refer to the FR Family Softune C/C_++ Compiler Manual for V6.
- Tags:
- fr81s family
-
This widget could not be displayed.Anonymous