Employee
Aug 10, 2020
02:37 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Aug 10, 2020
02:37 AM
FX3の電源投入シーケンス – KBA221826 - Community Translated (JA)
Community Translated by NoTa_4591161 Version: **
Translation - English: Power Up Sequence for FX3 – KBA221826
質問:
FX3には電源シーケンスがありますか?
回答:
FX3には電源投入シーケンスがありません。RESET_Nがアサートされる前に、すべての電源が安定していることを確認してください。すべての電源が1 msのリセット時間内に安定することを想定しています。したがって、RC回路を介して最低1 msのリセット時間を維持することをお勧めします。デザインで安定した電源を提供するのに1ミリ秒以上かかる場合は、リセット時間も増やす必要があります。
Rate this article: