Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

FR How to use well the sector protecting function

FR How to use well the sector protecting function

Anonymous
Not applicable

Answer:

FLASH sector protect function is to not erase programmed data to FLASH memory in order to protect data erase wrongly.
Sector protect is used parallel writer. Therefore at using sector protect function, please confirm the status to parallel writer maker (Flash Support Group Inc. and MINATO DEVICE COMPANY).

Example of procedure of Sector protect function

1.gif

1. Writes the boot program (Note 1) on the top sector by parallel programmer.
     (No erase anymore. ex; sector protection)
     Job before Flash MCU mounting
2. At the Flash memory Erase/Write mode, transfer the write/erase control program (Note 2) to internal RAM.
3. Executes the transferred Write/Erase control program.
     Write/Erase the Flash memory contents.

(Note 1)
A boot program is the program which transfer of the Write/Erase program to the internal RA.
Also, it can save the Write/Erase program.

(Note 2)
A Write/Erase program is the program which executes the Flash memory Write/Erase command.
(A operation of the Write/Erase program is the same as the externally connected MBM29F400T)

322 Views
Contributors