Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

FR How to make the efficient and high reliable C source. (Let's use C Checker)

FR How to make the efficient and high reliable C source. (Let's use C Checker)

Anonymous
Not applicable
Answer:

The Softune C Checker is a tool that accepts source programs written in C as input to point out the lines where quality and performance can be improved and to display and to print diagnostic messages useful in software development.

The C Checker assists in meeting the following needs:

Removes coding mistakes in early stages.
Gives new programs a thorough review in a short time.
Writes high-quality code (even for novices in C)
Write high-performance code.
Allows non-FUJITSU CPU software resources to be used with FUJITSU CPUs.
Understands the features of FUJITSU C compilers.

0 Likes
92 Views
Contributors