Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

FM4 MCUs: How the Output Impedance of the External Circuit Affects the ADC Sampling Time - KBA226795

FM4 MCUs: How the Output Impedance of the External Circuit Affects the ADC Sampling Time - KBA226795

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: TakashiM_61          Version: **

Community Translation: 外部回路の出力インピーダンスのADCサンプリングタイムへの影響 - KBA226795

 

The ADC Sampling time “ts” changes with the external impedance. You must ensure that the output impedance of the external circuit is fixed such that the following equation is satisfied, and meets A/D Converter Sampling time defined in the datasheet (for example S6E2H Series datasheet.)

Capture.JPG  

Where RAIN is the input resistance of the ADC, CAIN is the input capacitance of the ADC, and REXT is the output impedance of the external circuit.

pastedImage_27.png

For example, here is the ADC sampling time for FM4 Family S6E2H Series MCU according to the table Electrical Characteristics for the A/D Converter in the datasheet.

pastedImage_37.png

Minimum Sampling time is 0.3 µs if AVCC  ≥ 2.7 V , 1.2 µs if  AVCC  ≤ 2.7 V  .

Maximum Sampling time is 10 µs.

 

References of other FM4 Family device datasheets:

FM4 family products page

FM4 family datasheets

0 Likes
419 Views