Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

FM0+, FM3, and FM4: "Flash Erase" Command Erases CR Trimming Data

FM0+, FM3, and FM4: "Flash Erase" Command Erases CR Trimming Data

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Community Translation: FM0+、FM3およびFM4: 「フラッシュ消去」コマンドはCRトリミングデータを消去します

When the firmware in flash memory is upgraded, the flash memory needs to be erased once before re-writing the new firmware into flash. The Flash Erase (All Sector Batch Erase) command can be used to erase all sectors in flash.
However, the CR trimming data is stored in the flash memory for all FM0+, FM3, and FM4 family microcontrollers. Therefore, if the entire flash memory is erased by the Flash Erase command, the CR trimming data is erased, too.
The CR trimming data is located at different addresses depending on the device. Refer to the Flash Programming Manual and datasheet for each device in order to check the CR trimming data location. More here.

0 Likes
156 Views