- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
External Bus Interface in Traveo S6J3xxx MCUs - KBA226525
Author: kotaroh_86 Version: **
Translation - Japanese: Traveo S6J3xxx MCUの外部バスインターフェース‐KBA226525- Community Translated (JA)
Question 1:
In Traveo™ S6J3xxx MCUs, how will the External Bus Interface (EBI) work if the software accesses EBI address out of the area configured by SRAM/FLASH Address Control Register (EBI_SFADDCR0 to 7)?
Answer:
If the software accesses EBI address out of the area configured by SRAM/FLASH Address Control Register, then SFER bit of EBI ERROR Register (EBI_ERRR) is set to "1", and data abort occurs because EBI returns an error response to the internal bus.
Question 2:
When will the External Bus Interface (EBI) capture the MRDY (Memory Ready) signal as a wait state while connecting with a low speed device?
Answer:
The wait state of the MRDY signal is captured during the following timings synchronized with MCLK:
- When reading from the low speed device, MRDY signal is captured at the MCLK rising edge after the falling edge of MOEX (Read Enable)
- When writing to the low speed device, MRDY signal is captured at the MCLK rising edge after the falling edge of MWEX (Write Enable).
Note:
This KBA applies to the following series of Traveo MCUs:
- S6J3120
- S6J3300
- S6J3360
- S6J3370