- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Exporting EZ-PD™ PMG1 applications to IAR Embedded Workbench for Arm® (IAR EWARM) – KBA236734
Community Translation: EZ-PD PMG1 アプリケーションを IAR Embedded Workbench for ArmR (IAR EWARM) にエクスポートする KBA236734
Version: **
EZ-PD™ PMG1 applications can be developed using different third-party IDEs such as Keil uVision, and IAR Embedded Workbench for Arm®. This article describes the process of exporting EZ-PD™ PMG1 applications to IAR EWARM.
Prerequisites
- Project Creator (Included with ModusToolbox™ software)
- IAR Embedded Workbench for Arm® ver.9.30.1 or later
- PMG1 Development kit
Creating example program
1.Install IAR Embedded Workbench for Arm® ver.9.30.1 or later
2.Create a ModusToolbox™ application using the Project Creator tool
3. Open Project Creator tool. Click on PMG1 BSPs and PMG1-CY7110 BSP as shown in Figure 1
Figure 1 Select BSPs in Project Creator
4. Choose “IAR Embedded Workbench” from the Target IDE pull-down menu as shown in Figure 2 and click on Create option.
Figure 2 Choose IAR Embedded Workbench
5. Select Project > Create New Project > Empty project on the main menu and click OK as shown in Figure 3 and Figure 4
Figure 3 Create New Project
Figure 4 Create Empty Project
6. Browse to the ModusToolbox™ application directory, enter the desired application name, and click Save as shown in Figure 5
Figure 5 Select destination to save workspace file
7. Select File > Save Workspace after the application is created as shown in Figure 6. Then enter the desired workspace name
Figure 6 Save Workspace
8. Select Project > Add Project Connection and click OK
Figure 7 Add Project Connection
9. Select the .ipcf file on the Select IAR Project Connection File dialog and click Open as shown in Figure 8
Figure 8 Select IAR Project Connection File
10. Select Project > Make on the main menu.
Upon successful Build, the following message will be displayed in the log:
Figure 9 Build succeeded message in the log
To use KitProg3/Miniprog4:
- Select Project > Options > Debugger and select CMSIS-DAP in the Driver List; click OK
Figure 10 Select CMSIS DAP in Driver list
- Select Project > Download and Debug.
The debug window appears in IAR Embedded Workbench IDE as shown in Figure 11
Figure 11 Debug window in IAR Embedded Workbench IDE