- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Enabling/disabling CAPSENSE™ widgets in PSoC™ Creator - KBA233948
Community Translation: PSoC™ CreatorのCAPSENSE™ ウィジェットを有効化/無効化する - KBA233948
Version: **
You can use the following API functions and structure for the CAPSENSE™ component in PSoC™ Creator to enable/disable widgets. See the CAPSENSE™ component datasheet available as part of PSoC™ Creator installation for details.
Method 1: Using CapSense_SetParam() API
CapSense_SetParam(uint32 paramId, uint32 value);
where
- paramId = CapSense_WDGT_ENABLE<RegisterNumber>_PARAM_ID is the required register (see CapSense_RegisterMap.h)
- value = ‘0’: disable
value = ‘1’: enable
Bit masking is used to enable/disable a widget.
The following example has five CSD buttons configured:
Value takes a 5-bit value in the following format:
<Button4><Button3><Button2><Button1><Button0> (MSB = left-most bit, LSB = right-most bit)
Call the following function to enable only Button3 using value = 01000 (in binary) or 8 (in decimal):
CapSense_SetParam(CapSense_WDGT_ENABLE0_PARAM_ID, 8);
Call the following function to disable only Button2 using value = 11011 (in binary) or 27 (in decimal):
CapSense_SetParam(CapSense_WDGT_ENABLE0_PARAM_ID, 27);
Method 2: Using CapSense_SetupWidgetExt() API
CapSense_SetupWidgetExt (uint32 widgetId, uint32 sensorId);
where
- widgetId : ID of the widget (CapSense_<name>_WDGT_ID)
- sensorId : ID of the sensor present within the widget
After enabling the sensors using this API, CapSense_ScanExt() is used to scan the sensor. For example, to enable sensor0 of the Button0 widget, call the following function:
CapSense_SetupWidgetExt(CapSense_BUTTON0_WDGT_ID, CapSense_BUTTON0_SNS0_ID);
Method 3: Using the CAPSENSE™ RAM structure
The CapSense_dsRam structure is of CapSense_RAM_STRUCT struct type, and maintains various CAPSENSE™ parameters. To enable Button0 widget, use the following structure:
CapSense_dsRam.wdgtEnable[CapSense_BUTTON0_WDGT_ID] = 1;
To disable this widget, write ‘0’ to the wdgtEnable array.