Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Electrical Over-Stress (EOS) Review and FAQ

Electrical Over-Stress (EOS) Review and FAQ

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Electrical Over-Stress (EOS)

 

Electrical Over-Stress (EOS) is a term/acronym used to describe the thermal damage that may occur when an electronic device is subjected to a current or voltage that is beyond the specification limits of the device.

 

Get to know all about EOS in this article:

- EOS Damage;

- EOS Visual Damage;

- EOS External Damage;

- EOS Internal Damage; 

- Possible Causes of EOS;

- How to prevent EOS events;

Manufacturing Area ESD Control;

- Product/Application level;

- Causes of EOS Events in Manufacturing Area Operations;

- EOS F&Q;

 

An EOS event can be a momentary event lasting only milliseconds or can last as long as the conditions persist. EOS can be the result of a single non-recurring event or the result of ongoing periodic or non-periodic events.

ESD and EOS are related types of over-stress events but at opposite ends of a continuum of current/voltage/time stress conditions.

 

  • ESD is a very high voltage (generally >500V) and moderate peak current (~1A to 10A) event that occurs in a short time frame (generally <1µs).

  • EOS is a lower voltage (<100V) and large peak current (>10A) event that occurs over longer time frame (generally >1ms).

Latch-up occurs when the device reaches a threshold (current and voltage) that causes a parasitic SCR structure to turn ON. Once turned ON, the latch-up condition will persist until the supply voltage is removed. Latch-up can create EOS damage if the current is large and/or if it persists over a long period.

The electrical failure in the customer’s application may show one or more of the following symptoms:

 

  • Excess supply current
  • Low resistance between the supply voltage and ground
  • Shorted input or output pins to either the supply voltage or ground
  • Open connections to one or multiple pins – I/O, supply voltage, or ground
  • Functional failure due to internal damage to the device

EOS Damage

 

The thermal damage is the result of the excessive heat generated during the EOS event.

The heat is a result of resistive heating in the connections within the device. The high currents experienced during the EOS event can generate very localized high temperatures even in the normally low resistance paths. The high temperature causes destructive damage to the materials used in the device’s construction.

Visual Damage

 

EOS damage can at times be seen as visual damage to the device. This damage is the result of the high temperatures experienced during the EOS event.

External (visible to the naked eye or with low power microscope):

  • Visible bulge in mold compound
  • Physical hole in mold compound
  • Burnt/discolored mold compound
  • Cracked package

Internal (visible after decapsulation with high-power microscope):

  • Melted or burnt metal
  • Carbonized mold compound
  • Signs of heat damage to metal lines
  • Melted or vaporized bond wires

EOS External Damage

 

               Package Bulge                                                Package Hole                                  Package Burnt/Cracked

pastedImage_0.png     pastedImage_1.png     pastedImage_2.png

 

EOS Internal Damage

 

                        Burnt Metal                                                    Open Connection                                            

pastedImage_3.pngpastedImage_4.png

                      

                        Heat Stress                                                 Melted Bond Wire

pastedImage_5.pngpastedImage_6.png

 

Possible Causes of EOS

 

  • Uncontrolled voltage surge on the power supply.

  • Voltage spikes due to internal PCB switching.

  • Voltage spikes due to an external connection – capacitive charge on an external cable, antenna pick-up of external switching noise, inductive loads.

  • Poor grounding resulting in excessive noise on the ground plane.

  • Overshoot or undershoot during I/O switching.

  • EMI (electromagnetic interference) due to poor shielding in an electrically noisy environment.

  • ESD events that trigger a larger EOS event or cause damage that weaken the device making it more susceptible to future EOS events.

  • Latch-up events may result in EOS damage if the current is high or if it persists for an extended period.

  • Connecting external cable to an unprotected I/O port

How to Prevent EOS Events

 

Manufacturing Area ESD Control

  • Proper use of conductive flooring and workspaces.

  • Proper use of personnel grounding straps.

  • Proper cart and shelving grounding.

  • Proper checking of solder rework equipment for EM leakage.

  • Proper control of humidity levels in work areas.

Product/Application Level

 

  • Clean Vcc and Vss supplies

  • Controlled Vcc ramp at power up and power down

  • Proper power/ground de-coupling capacitors

  • Data buss contentions

  • PCB low-resistance conduction paths for power and ground

Causes of EOS Events in Manufacturing Area Operations

 

  • Poor test equipment grounding

  • Multiple ground connections

  • Ground loop currents

  • Mix-ups between Chassis ground and electrical safety ground

  • AC power line surges (large switching currents)

  • Inductive/Capacitive loads

  • Connecting long cables to active circuits

  • Damaged or poorly maintained sockets on programmers

  • Incorrect insertion into programmer sockets

  • Component board mounted in wrong orientation

Electrical Over Stress (EOS) FAQ

 

What is EOS?

 

- EOS is thermally induced damage to a component induce by an overvoltage condition.

How different is EOS from ESD?

 

- EOS and ESD are related voltage overstress conditions but they differ in the total energy and time span of the event. EOS has higher energy and a longer time span.

How to prevent EOS?

 

- A careful review of the power supply variations and input signals to look for possible conditions that exceed the product specifications.

Does Infineon test for EOS?

 

- No. There are currently no industry standards that allow for testing for EOS type conditions.

Are EOS and Latch-up the same?

 

- No. Latch-up is a specific event that occurs when the parasitic SCR device is triggered, while EOS is a general description of any electrical overstress. EOS may not be caused by Latch-up and Latch-up can occur without causing permanent EOS damage to the component.

Does Infineon has a specification for EOS tolerance?

 

- No. Infineon tests for ESD and Latch-up per JEDEC standards. See Infineon's web site for more information on the product qualification requirements.

Does Infineon have specific PCB layout rules to prevent EOS?

 

- No. EOS is an event that can occur on any PCB layout.

What process parameter will cause EOS tolerance to degrade or improve?

 

- Infineon tests all products to function properly under the specification limits. An EOS event is an event that occurs outside the specification limits.

How to detect an EOS problem in the field?

 

- An EOS damaged component may exhibit excessively high current or low resistance between power and ground.

Why is Infineon's component the only part failing on the board?

 

- Normally, in an EOS event, more than one component will experience the voltage surge. However, based on placement and electrical connections on the PCB and sensitivity of the components, one component will fail first and the current will be shunted to that component, resulting in more damage that component.

The power supply is clean. How to understand that the Vcc damage is a customer problem?

 

- Variations in the Vcc supply or ground can be non-periodic and be influenced by external conditions. A limited-time review of the voltage supply may not reveal the problem. Monitoring the supply voltage over a longer time and with properly set trigger levels may reveal the problem if the issue is periodic in nature. If, however, the EOS was triggered by non-recurring event then monitoring the supply voltage may never reveal the problem. 

I/O signals have small/no over/under shoot. How can you still have EOS damage?

 

- Variations in the I/O signal can be non-periodic and be dependent on external and internal switching. It is possible for large spike on the I/O pin to cause a latch-up event. This event, if not terminated, may cause thermal damage to the component. Monitoring the I/O voltages over an extended time with properly set trigger levels may reveal voltage spikes that can cause a component to fail.

Damage caused by EOS

 

- The damage caused by EOS is typically so extensive that the origin of the problem cannot be determined. An initial small voltage perturbation can cascade into a large event and cause damage that overwhelms the original damage site. The analysis report will identify which package pins are damaged and with this information you should be able to identify potential areas for further investigation such as power supplies or I/O signals.

Isn’t this Infineon's design/process/manufacturing problem?

 

- Infineon's designs and tests its parts to function within the specified operating parameters. We also qualify our parts using industry standard test methods including ESD and Latch-up. Qualification data is available on the Infineon's web site, Infineon.com.

However, all semiconductor components will eventually fail if exposed to conditions beyond the datasheet specifications. EOS damage cannot be generated by the internal conditions of the component when operating within the datasheet specifications. The EOS damage can only occur when abnormal external conditions are present.

 

Additional Information

Additional Information is available at Infineon's web site. General product information and datasheets are available at:

Infineon's Corporate Web site: https://www.infineon.com/

Infineon's Corporate Quality web site: Infineon corporate quality web-site

 

Reference Information

The following is a list of other resources located on various web sites.

“White Paper 4 - Understanding Electrical Overstress – EOS” from Industrial Council on ESD Target Levels, August 2016.

This document is available through various public domains as listed below:

The ESD Association is a very good resource for learning or training on ESD and EOS. The association has an annual symposium dedicated to ESD and EOS.

ESD Association – www.esda.org

  • Annual EOS/ESD Symposium
  • Classes/Books on ESD and EOS

The following web sites discuss EOS. A general search of the web will find many more references.     

www.bestesd.com/library/Origins-of-EOS.pdf

www.ce-mag.com/archive/02/Spring/dangelmayer.html

 

Version: *B

Translation - Japanese: 電気的オーバーストレス(EOS)のレビューとFAQ - KBA225846 - Community Translated (JA)

0 Likes
21373 Views
Contributors