Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Elderly Fall Detection

lock attach
Attachments are accessible only for community members.

Elderly Fall Detection

MatthewS_51
Employee
Employee
50 questions asked 10 likes received 10 questions asked

This project was submitted by R.M. Dreifuerst in Make With Mesh: The Cypress & Digi-Key Bluetooth 5 IoT Design Contest Sponsored by Embedded Computing Design and was one of the winners!

 

pastedImage_3.png

 

Project Technology Focuses

  • CYW20819 Dual-Mode Bluetooth 5 MCU
  • Machine Learning

 

Project Requirements

Hardware

  • CYW20819 Arduino Eval Kit (CYW920819EVB-02)
  • Additional button for forced fall detection

Software

 

Project Description

This project leverages the CYW20819 Arduino Eval Kit to implement a machine learning powered automatic fall detection IoT device. Providing a fast and early response to medical emergencies is one of the most effective methods of ensuring recovery from hazardous situations - and so adding some automation to this process certainly brings to light some of the benefits in the medical world the IoT can bring. The project first created a data pipeline with the desired "fall" output using the on-board accelerometer on the CYW20819. The data was then fed into multiple machine learning models - eventually with a tested model being migrated to run on the CYW20819 processor to do automatic fall detection. In the end version of this project, if a fall is detected an emergency call on the user's smartphone would be initiated via Bluetooth.

pastedImage_23.png

 

Project Links

 

Resource List

Attachments
0 Likes
774 Views