cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Eclipse IDE for ModusToolbox Quits Unexpectedly on macOS Big Sur - KBA233132

Chelladurai
Community Manager
Community Manager

Eclipse IDE for ModusToolbox Quits Unexpectedly on macOS Big Sur - KBA233132

Version: **

Question:
Why did the Eclipse IDE for ModusToolbox quit unexpectedly on my macOS Big Sur machine?
Answer:
For some macOS machines running on M1 processors, the Eclipse IDE may fail to start with a message such as:

"ModusToolbox quit unexpectedly."

The message details also state that the "attachment of code signature supplement failed."
This problem occurs any time that Eclipse was last opened in an empty workspace prior to a reboot. After the reboot, the application fails to start.
Run the following command in the /Applications/ModusToolbox/ide_x.y/ModusToolbox.app directory:

xattr -dr com.apple.quarantine *

Note:
You may have to adjust the path if you installed ModusToolbox in a non-default location. 
When complete, launch the Eclipse IDE again. This workaround works for all cases so far discovered.

 

 

 

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎May 03, 2021 11:00 PM
Updated by:
 
Contributors