Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

EZ-USB®FX3S™のPからUチャネルでの最大スループット – KBA90896 - Community Translated (JA)

EZ-USB®FX3S™のPからUチャネルでの最大スループット – KBA90896 - Community Translated (JA)

IFX_Publisher1
Community Manager
Community Manager
Community Manager
250 sign-ins First comment on KBA 250 replies posted

EZ-USB®FX3S™のPからUチャネルでの最大スループット – KBA90896 - Community Translated (JA)

Community Translated by NoTa_4591161      

Version: *A

Translation - English: Maximum Throughput on the P to U Channel in EZ-USB® FX3S™ – KBA90896

 

質問: FX3S™PからUチャネルの最大スループットはどのくらいでしょうか?

回答:

FX3Sは、最大100 MHzで動作するGeneral Programmable InterfaceGPIF)で16ビットのデータバスを使用します。ここでは、理論上の最大値は200 MBps、つまり100 MHz * 2バイトです。実際のテストでは、187 MBpsの結果が示されています。

注: FX3SGPIFデータ幅は、8ビットまたは16ビットのいずれかです。最大のスループットを得るには、16ビットに構成する必要があります。

0 Likes
94 Views