ESD Level for GPIOs of PSoC® devices - KBA98298
Anonymous
Not applicable
Oct 25, 2016
01:36 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Oct 25, 2016
01:36 AM
Version: **
Translation - Japanese: PSoC®デバイスのGPIOのESDレベル - KBA98298 - Community Translated (JA)
Question:
What is the ESD acceptance level on GPIO pins of PSoC devices?
Answer:
The ESD acceptance level of the GPIOs of all PSoC devices is 2 kV Human Body Model (HBM). For more information, see the Absolute Maximum Ratings section of the device datasheet. The device datasheets can be found here.
Labels
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous