Community Manager

Community Manager
Jun 28, 2022
11:59 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
E-marking on USB Type-C Cables: When is it required ? (KA-03260)
E-marking (having a Type-C controller) for the Type-C to Type-C cable is required under the following conditions:
- If the Type-C cable is required to support more than 3A current
- If the Type-C cable is a full featured cable i.e, if the cable either supports either USB 3.1 Gen1 or USB 3.1 Gen2 signaling
More https://community.infineon.com/t5/Knowledge-Base-Articles/E-marking-on-Type-C-Cables-KBA98430/ta-p/2... here.
Labels
Rate this article: