Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Drive Capability of LVDS Port in Traveo S6J3200 Series MCUs – KBA227497

Drive Capability of LVDS Port in Traveo S6J3200 Series MCUs – KBA227497

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: ShusakuS_56   Version: **

Translation - Japanese: Traveo S6J3200シリーズMCUのLVDSポートのドライブ機能 - KBA227497 - Community Translated (JA)

Question:

What is the drive capacity of the LVDS port in the S6J3200 series?

Answer:The drive capability of LVDS can be set to either 300 mV, 350 mV, or 400 mV. Drive Capability is switched by the Control1 Registers (CTRL1 register). For more details, refer to FPD-Link Converter section in the TRM from the following link.

- https://www.cypress.com/documentation/technical-reference-manuals/32-bit-microcontroller-traveo-fami...

0 Likes
311 Views
Contributors