Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Does SEMPER™ NOR Flash of Endurance Flex require any configuration setting in your system?

Does SEMPER™ NOR Flash of Endurance Flex require any configuration setting in your system?

YukaA_81
Employee
Employee
5 solutions authored 10 replies posted First like given
  • In the default setting, all areas (except 4KB sector) are set to High Endurance/Wear leveling Enable.
  • If there is a combination of areas that require data retention with low endurance (e.g. Boot code) and areas that require high endurance (e.g. Data Logging), the areas that should have low endurance will be targeted for Wear Leveling and may not meet your data retention requirements.
  • The Endurance Flex feature in the SEMPER™ NOR Flash Series requires settings that are suitable for your system's usage.
  • Endurance Flex feature can be configured with the Endurance Flex Architecture Selection Register (EFXx).
  • The Endurance Flex Architecture Selection Register (EFXx) consists of One Time Programmable bits, so these bits cannot be changed once set. In addition, please do not change the settings after release to the end customer.
0 Likes
101 Views